When do I need to use a LAN/GPIB Gateway (Option 011) with my EMI Measurement System?
A LAN/GPIB Gateway is only required when using an alignment signal source without a LAN connection. Of the support signal sources the only one that does not have a LAN connection is the 8648B.