How do I use my 1680/1690/16900-series logic analyzer without entering a username and password?
By default, the Windows 2000 and Windows XP operating systems in these machines require users to log in with a user name and password. You may wish to change this behavior to make the analyzer more easily accessible to yourself and others. This is possible if your analyzer is not a member of a Windows domain.
Follow this procedure to remove the login prompt from the Windows startup sequence. You can determine your version of Windows by clicking Start | Run and entering the winver command.
Windows XP machines
- Click Start | Run and type sysdm.cpl. Click OK.
- Click the Computer Name tab.
- Look under "Full computer name:". If you see "Workgroup:", your machine does not belong to a domain and you may proceed to step 4. If you see "Domain:", click Change... and select "Workgroup:" under "Member of". You will need to name a workgroup (this can be an arbitrary name). Please be aware that leaving a domain may limit your access to certain network resources. Reboot your machine if prompted.
- Click Start | Run and type control userpasswords2. Click OK.
- Clear the "Users must enter a username and password to use this computer" check box and click Apply.
- Enter the user name and password for the account to which Windows will automatically log on upon startup. The default account is Administrator with a blank password.
- Click OK twice. The next time you reboot you should not be prompted for a user name or password.
Windows 2000 machines
- Click Start | Run and type sysdm.cpl. Click OK.
- Click the Network Identification tab.
- Look under "Full computer name:". If you see "Workgroup:", your machine does not belong to a domain and you may proceed to step 4. If you see "Domain:", click Properties and select "Workgroup:" under "Member of". You will need to name a workgroup (this can be an arbitrary name). Please be aware that leaving a domain may limit your access to certain network resources. Reboot your machine if prompted.
- Click Start | Run and type control userpasswords. Click OK.
- Clear the "Users must enter a username and password to use this computer" check box and click Apply.
- Enter the user name and password for the account to which Windows will automatically log on upon startup. The default account is Administrator with a blank password.
- Click OK twice. The next time you reboot you should not be prompted for a user name or password.