Why do I get verification error upon reset with single channel pulsed switches and Y1151A distribution board?
On this particular distribution board, sending "ROUTe:RMODule:BANK:PRESet {
Workaround: if you want to drive a pulsed switch channel closed at reset using the Y1151, you should send a "ROUTe:CHANnel:DRIVe:OPEN:DEFault (@ channel 7)" to put the open all port on the switch into a state that won't get pulsed by default, and then send "ROUTe:CHANnel:DRIVe:CLOSe:DEFault (@user channel)" so that the desired channel closes automatically at reset.