How do I transfer trace data to a PC from a CSA using VEE?
The examples below demonstrate the use of the remote commands for transferring trace data from the instrument. These can be downloaded and run using VEE 7.0 or later. If you are not using VEE and you would like to see what instrument remote commands are required to do this you can view the image files instead for a look at what the program contains.
There are two example that can be downloaded. One is a simple example that only transfers the trace data itself. The other also uses instrument parameters to configure the data display according to its current settings.
If you do not currently have a copy of Keysight VEE, you can go to the VEE web site to find out more about it as well as download a free 30 day trial version: