What are the measurement intervals for the W-CDMA, cdma2000, and 1xEV-DO QPSK EVM measurements for E4406A and the PSA Series? Is the 12.2k Reverse ...
In the A.04.07 release of the PSA Series firmware and the A.06.03 release of the E4406A, the measurement intervals for the QPSK EVM measurement as follows:
- cdma2000 (Option B78) - 128 to 1536 chips
- W-CDMA (Option BAF) - 128 to 2560 chips (1 slot)
- 1xEV-DO (Option 204) - 32 to 2048 chips
The W-CDMA personality does support uplink 12.2 k RMC (Reverse Measurement Channel) in the QPSK EVM measurement.