For the 4395A / 4396B combination analyzer in spectrum analyzer mode with the noise format. Are the indicated units in error for this mode?
Due to 4395A / 4396B display limitations, the screen annotations are unable to correctly indicate the desired units of 'nV / √Hz'.
The limitations are documented within the related manuals as follows:
4395A:
Refer to the Keysight 4395A Network/Spectrum/Impedance Analyzer Operation Manual , 'Measuring the Noise Level', page 8-36 and the following excerpt:
4396B:
Refer to the Keysight 4396B Network/Spectrum/Impedance Analyzer Task Reference, 'Measuring the Noise Level', page 3-3 and the following excerpt: