您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

示波器、分析儀、儀錶

1-16 / 16

排序:
Introducing SystemVue 2016
See a live demo of SystemVue 2016. The new capabilities enable researchers and system architects working on platforms using beamforming algorithms for 5G, satellite, NewSpace, radar and EW applications, to reduce interference and power consumption, while increasing physical range.

基本展示 2016-06-27

NewSpace and Traditional Space panel session– recorded at the NewSpace 2015 conference
Streamed live on July 16, 2015, this video is a panel discussion of important key players in the NewSpace arena.

基本展示 2016-02-02

Precision Validation of Radar System Performance in the Field Using FieldFox

基本展示 2014-03-21

Realistic Ultra Wideband Radar Signal - Demo
Testing of radar systems can be extremely time-consuming and expensive. Radar transceivers must be designed and tested with realistic environment and jamming scenarios, which often involve costly outdoor ranges, chambers, and real-time hardware simulators.

基本展示 2013-11-25

EVM measurement with the new M8190A Arbitrary Waveform Generator - video
To meet the high demands of aerospace/ defense application tests, it is indispensable to simulate real-life scenarios with precision arbitrary waveforms. In a test setup with a high error vector magnitude (EVM), problems within your device under test may not be discovered. With signals close to reality, the Keysight M8190A is the perfect solution.

基本展示 2012-08-20

Reconfigurable Radar Design: Debug and Validation - video
This video demonstrates how to debug and validate reconfigurable radar design with Keysight test and measurement instruments and software.

基本展示 2012-07-30

Interference Mitigation Through the Use of Wideband Signal Recording and Analysis - video
This video describes the process to find and analyze the cause of a radio signal that is interfering with a wireless LAN transmitter. This requires the continuous capture of wireless spectrum, tools to search and find possible interferers as well as tools to determine how an interferer may affect the LAN signal.

基本展示 2012-06-11

WMF WMF 33.25 MB
OFDMA Concepts Demonstration - channel training sequence - video
This video describes one of the key concepts of Orthogonal Frequency Division Multiple Access (OFDMA) modulation. This video illustrates how a channel training sequence can be used to discern two distinct transmission streams in a MIMO (Multiple In Multiple Out) Antenna configuration.

基本展示 2012-06-11

WMF WMF 20.57 MB
Microwave Switch Repeatability Demonstration - video
This video compares the repeatability performance of a Keysight microwave switch with a competitor’s offering. Performance is compared by measuring the insertion loss across a frequency range, then comparing the relative difference of each insertion loss measurement.

基本展示 2012-06-11

WMF WMF 17.78 MB
OFDMA Concepts Demonstration - channel training sequence - video
This video describes one of the key concepts of Orthogonal Frequency Division Multiple Access (OFDMA) modulation. This video illustrates how a channel training sequence can be used to discern two distinct transmission streams in a MIMO (Multiple In Multiple Out) Antenna configuration.

基本展示 2012-05-10

Reproducing DC Power Transients, Using an N6705B DC Power Analyzer to Create Transients - video
DC power transients can easily be reproduced with N6705B DC Power Analyzer. Power transients can be used to test a DUT resilience to a change in voltage. Two examples are provided an automobile's voltage during engine turn-on and a PS interrupt specified in the DO-160F avionics test manual. Transients can also occur when the load on a PS changes.

基本展示 2012-05-10

Measuring Performance of Wide Bandwidth Radar Transmitters
Short videos on measuring performance of wide bandwidth radar transmitters.

基本展示 2011-04-21

Self-diagnosing Switch Matrix
Self-diagnosing Switch Matrix

基本展示 2011-02-16

Signal Studio for Global Navigation Satellite Systems N7609B Video Demonstrations
View this series of three videos which will provide an introduction to the N7609B Signal Studio for Global Navigation Satellite Systems (GNSS) software and demonstrates some of the key features of the software.

基本展示 2010-03-30

P-Series Power Meter Radar Video Demonstrations

基本展示 2009-04-01

E3238S / 35688E Product Tour DVD

基本展示 2006-11-28

PDF PDF 185 Bytes