您可能感興趣的網頁。 觀看搜尋結果:

 

聯絡是德專家

軟體

下載軟體,即享前瞻洞察力。Get a Free Trial

是德科技將種類眾多的不同應用軟體,整合為一套簡單的多功能版本,讓您能輕鬆快速地獲得所需的專業知識與洞察力。是德科技軟體讓專業量測知識唾手可得。從第一次模擬,到第一次出貨,我們在整個流程中提供包羅萬象的量測工具,以加速您獲得量測資料、解析重要資訊,並制訂執行方案。我們的產品涵蓋從 ADS 與 VSA 等暢銷版本,一直到可因為未來技術的先進軟體。只要下載軟體,您可隨時獲得精湛洞察力。

  • 我們領先業界的電子設計自動化軟體(EDA)可加速射頻、微波與高速數位設計的開發
  • 嵌入式和單機板軟體可協助您進行更深入的量測與分析
  • 利用功能強大的工具程式,省時省力地完成從簡單連接到編程控制的各項作業
  • 程式設計環境包括圖形程式設計、排序和分析套件
     

立即申請免費的試用版軟體

獲得是德科技軟體管理的詳細資訊。
 


獲得是德科技軟體的詳細資訊

Design & Test Software Video - by Keysight Industry Expert

是德科技設計與測試軟體概述 

了解是德科技設計和測試軟體如何協助您節省時間和精力、做出更好的決策、加速完成設計,並且簡化工作流程。

Video which demostrates simulate designs, analyze signals with Keysight Software

使用是德科技軟體進行設計模擬、信號產生與分析等任務 

了解是德科技軟體可在一分鐘內完成的任務。

是德科技軟體讓專業技術觸手可得 

20 秒獲得量測洞察力。立即使用是德科技軟體開始進行量測。

1-25 / 52

排序:
Using MATLAB to Create Keysight Signal and Spectrum Analyzer Applications - Application Note
Learn to use MATLAB software to configure, control, and acquire data from X-Series signal and spectrum analyzers, and then use scripts to create, modify and execute custom analyzer applications.

應用手冊 2016-11-16

PDF PDF 9.69 MB
Spectrum Analysis Basics - Application Note
This application note (also known as AN 150) explains the fundamentals of swept-tuned, superheterodyne spectrum analyzers and discusses the latest advances in spectrum analyzer capabilities.

應用手冊 2016-11-02

New Pulse Analysis Techniques for Radar and EW - Application Note
This app note discusses the best tools for different types of pulse analysis, along with display and analysis techniques for various signals and measurement goals.

應用手冊 2016-05-26

Radar Development Using Model-Based Engineering
This application note describes how SystemVue is well suited for use in model-based engineering. It is for system engineers, directors of engineering and people involved in the development of Radar.

應用手冊 2015-04-14

PDF PDF 1.59 MB
Generating Multi-Dimensional Signals to Test Radar/EW Systems
This application note describes how to use SystemVue to generate multi-dimensional signals for testing Radar and modern Electronic Warfare (EW) systems.

應用手冊 2014-11-09

GNSS(全球衛星導航系統)技術和接收機測試 - 應用說明
全球衛星導航系統(GNSS)泛指使用衛星信號來確定用戶接收器位置的系統。目前的全球衛星定位系統(GPS)中,美國的 GPS 系統和俄國的GLONASS 系統皆已全面運作,可提供全球定位服務。此外,中國的北斗(Beidou)系統(也稱為 Compass)和歐盟的 Galileo 系統也正加速部署。

應用手冊 2014-08-30

Radar Measurements - Application Note
This application note focuses on the fundamentals of measuring basic pulsed radars and measurements for more complex or modulated pulsed radar systems.

應用手冊 2014-08-22

PDF PDF 6.84 MB
Analyzing Frequency Stability in the Frequency and Time Domains - Application Note
Describes both methods with an emphasis on practical, cost-effective solutions. For those who are new to the time-domain perspective, two proven frequency-to-time conversion methods are also presented.

應用手冊 2014-08-11

Simulation and Verification of Pulse Doppler Radar Systems - Application Note
Keysight SystemVue illustrates key algorithms in modern Pulsed Doppler radar system design, and also connects to Keysight sources and signal analyzers to verify hardware performance.

應用手冊 2014-08-02

PDF PDF 10.44 MB
Using Flexible Digital Modulation Testing for Satellite Regenerative Payloads - Application Note
This application note focuses on solutions for the issues that create risks in the integration of mixed-signal systems with a mix of software and hardware tools. Examples focus on measurements of error vector magnitude (EVM), which is a key figure of merit for modulated signals implemented in either analog or digital form.

應用手冊 2014-08-01

FPGA Prototyping Using Keysight SystemVue
This application note describes a top-down FPGA design flow using SystemVue for rapid prototyping of physical layer communications signal processing.

應用手冊 2014-08-01

Overcoming the Challenges of Simulating Phased-Array Radar Systems
This application note discusses a solution that reduces design cycles, significantly reduces cost and allows you to simulate a scenario before taking it to land, skies and seas.

應用手冊 2014-02-26

Creating Multi-Emitter Signal Scenarios with COTS Software and Instrumentation – Solution Brief
Describes a key problem, describes a commercial, off-the-shelf (COTS) solution for signal generation and analysis, and presents two example scenarios.

應用手冊 2013-11-12

PDF PDF 1017 KB
Cost Savings in Creating Realistic Multi-Emitter Signal Scenarios
Describes a commercial, off-the-shelf (COTS) solution for signal generation and analysis, and presents two example scenarios.

應用手冊 2013-05-02

Radar, EW & ELINT Testing: Identifying Common Test Challenges - Application Note
This application note reviews some of the latest test equipment for radar, EW & ELINT systems. Since this is a complex subject, we begin with a brief review of the fundamental radar and EW/ELINT challenges.

應用手冊 2013-04-29

Make Custom OFDM Measurements with 89600 VSA Software Option BHF - Application Note
Read about how to configure 89600 VSA software with Option BHF custom OFDM modulation analysis to analyze and troubleshoot new, custom, proprietary, generic, or non-standard OFDM signals.

應用手冊 2012-11-21

PDF PDF 4.27 MB
Designing, Verifying and Testing Stepped Frequency Radar Systems for Commercial and A/D Applications
This note shows a simulation platform using SystemVue software that easily links measurement tools to enable the design, validation and test of SFR systems under different environments.

應用手冊 2012-10-18

PDF PDF 688 KB
Using Keysight SystemVue to Create Realistic Scenarios for Radar and EW Applications
Shows how the combination of software and hardware capabilities makes it possible to create dynamic and realistic scenarios for both component testing and scenario simulation for system test.

應用手冊 2012-01-24

Making Wideband Measurements - Application Note
This paper will discuss using the Keysight PXA signal analyzer as a microwave down converter for an Infiniium oscilloscope or Acqiris digitizer running the 89600 VSA software.

應用手冊 2012-01-24

High-Power Measurement Using The E5072A Network Analyzer Application Note
This application note describes how to make high-power measurements with unique functions of the E5072A network analyzer.

應用手冊 2011-12-23

Application of Keysight's PNA-X NVNA and X-Parameters in Power Amplifier Design
This 16-page article appeared in Microwave Journal's May 2011 issue; teaches you how to obtain actual linear and nonlinear component behavior to improve power amplifier design using Keysight's solutions.

應用手冊 2011-05-01

Using SystemVue’s Radar Library to Generate Signals for Radar Design and Verification - App Note
Keysight's Radar Library helps you with the productivity and accuracy of your radar signals.

應用手冊 2011-01-25

Custom OFDM Signal Generation Using SystemVue - Application Note
This application note describes a new comms standard based on OFDM which is provided by SystemVue 2011 to create both simulation and measurement, with links to the new 89600B VSA software for further demodulation and analysis.

應用手冊 2010-12-09

Combining Simulation and Test to Accelerate SDR Development
The note reviews the major attributes of SDRs then looks at two key topics: the use of multiple waveforms during SDR design and the use of simulation to add flexibility to SDR testing.

應用手冊 2010-11-19

PDF PDF 2.22 MB
Typical GPS Receiver Verification Tests Using a GPS Signal Simulator - Application Note
This paper describes typical GPS receiver verification tests using a GPS signal simulator. The tests are used to verify functionality of embedded GPS receivers in mobile consumer products such as cell phones and other handheld receivers.

應用手冊 2010-03-04

1 2 3 下一頁