Contact an Expert

Thread: Error 801 Configuration Error Problems


Permlink Replies: 1 - Pages: 1 - Last Post: Aug 12, 2012 10:54 PM Last Post By: changmeikuan Threads: [ Previous | Next ]
StevenH

Posts: 2
Registered: 08/10/12
Error 801 Configuration Error Problems
Posted: Aug 10, 2012 6:36 AM
Click to report abuse...   Click to reply to this thread Reply
Attachment Error 801.bmp (227.8 KB)
Agilent,

I have been working on an old program created originally in Vee 6.0 and now trying to run on runtimes of 7.5 or newer and have been running into and issue with a configuration error.

When the program begins and trys to use any of the intrument panels is pops up with a configuration error: Driver for "RF_Gen" not found. RF_Gen being the manual identifier. It is saying that it wants ID filename hp8647_8.cid which i added to the ids folder of the runtime in the C:\program files\agilent\agilent vee runtime x.x

When running in the development environment there is no problem.

checked that the driver is not located in another location. not sure why i am running into this issue. any help would be great.
changmeikuan

Posts: 210
Registered: 08/07/09
Re: Error 801 Configuration Error Problems
Posted: Aug 12, 2012 10:54 PM   in response to: StevenH in response to: StevenH
Click to report abuse...   Click to reply to this thread Reply
Go to Start > Programs > Agilent VEE Pro xx RunTime Config and launch IO Configuration. Add the instrument used in the program there, with the same name and also set the Panel Driver file. This should fix the problem I hope :)

Hope this helps,
  • mk

Point your RSS reader here for a feed of the latest messages in all forums