Contact an Expert

Thread: Signal Studio For Bluetooth (N7606B)


Permlink Replies: 2 - Pages: 1 - Last Post: Aug 29, 2012 9:20 AM Last Post By: tabbott
aoran_youran

Posts: 2
Registered: 08/09/12
Signal Studio For Bluetooth (N7606B)
Posted: Aug 9, 2012 9:48 PM
Click to report abuse...   Click to reply to this thread Reply
I am using Agilent Signal Studio for Bluetooth to generate waveform for sensitivity test. What I expected is 10 packets and each contains payload. But the result is 20 packets and only first 2 contain payload data. First packet contains 2712 (full packet) bits and second one contains 1376 (1376=511*8-2712) bits. How should I do to reach my target?
aoran_youran

Posts: 2
Registered: 08/09/12
Re: Signal Studio For Bluetooth (N7606B)
Posted: Aug 19, 2012 9:24 PM   in response to: aoran_youran in response to: aoran_youran
Click to report abuse...   Click to reply to this thread Reply
The version I used is 3.3.2.0. I tried an older version 1.0.0.0 and the generated waveform is better, in which every packet contains payload data. Unfortunately, when dirty is on LAP address (which determines syncWord value) doesn't take effect. I tried input different LAP address, syncWord keeps same. However if dirty is off, I can get the syncWord value which is I wanted.
Can anybody help? Or can anybody tell me where I can get other versions then I can try?
tabbott


Posts: 1,483
Registered: 07/24/09
Re: Signal Studio For Bluetooth (N7606B)
Posted: Aug 28, 2012 5:28 PM   in response to: aoran_youran in response to: aoran_youran
Click to report abuse...   Click to reply to this thread Reply
Hi -

We hope you are happy with the setup file you received.

Regards -

Edited by: tabbott on Aug 29, 2012 9:19 AM

Point your RSS reader here for a feed of the latest messages in all forums