Contact an Expert

Thread: 33522A LAN issues and units locking up


Permlink Replies: 1 - Pages: 1 - Last Post: Aug 10, 2012 4:42 PM Last Post By: cldiller Threads: [ Previous | Next ]
Aaron

Posts: 1
Registered: 07/24/12
33522A LAN issues and units locking up
Posted: Jul 24, 2012 10:26 AM
Click to report abuse...   Click to reply to this thread Reply
We have about twenty 33522A units in our development area and half of them are experiencing random lock-ups that only a power-cycle can break. These same units do not respond to ping requests when setup with static IPs, and when the LAN is configured for DHCP they either don't come up with and IP address information or come up with 169.X.X.X addresses (which is not in any of our subnets).

Those units that are experiencing the LAN configurations are also experiencing the lockups, a device that has never been connected to the network appears to have no issues whatsoever.

Since LAN connectivity is down, this makes upgrading (or for that matter, just reloading) the firmware impossible since the only firmware upgrade we know about is done over the network. Is it possible to perform any diagnostics or firmware upgrades without LAN connectivity?

cldiller

Posts: 23
Registered: 08/05/09
Re: 33522A LAN issues and units locking up
Posted: Aug 10, 2012 4:42 PM   in response to: Aaron in response to: Aaron
Click to report abuse...   Click to reply to this thread Reply
Hi, Aaron,

Do you experience the same problems when using a manual IP address?

Point your RSS reader here for a feed of the latest messages in all forums