Contact an Expert

Thread: Help on the warning "No objects selected" in ADS2011 schematic environment


Permlink Replies: 5 - Pages: 1 - Last Post: Jul 21, 2012 7:28 AM Last Post By: AaronHe
AaronHe

Posts: 3
Registered: 07/07/12
Help on the warning "No objects selected" in ADS2011 schematic environment
Posted: Jul 7, 2012 10:32 PM
Click to report abuse...   Click to reply to this thread Reply
In ADS2011 schematic environment, the warning "No objects selected" will come out from time to time.
This is really annonying.
Is there any method to ignore this warning?
Thanks a lot!
eyeung

Posts: 50
Registered: 01/22/09
Re: Help on the warning "No objects selected" in ADS2011 schematic environment
Posted: Jul 13, 2012 6:00 PM   in response to: AaronHe in response to: AaronHe
Click to report abuse...   Click to reply to this thread Reply
Your best bet is to contact your local technical support to resolve this issue.
ADSProductManager

Posts: 7
Registered: 07/09/12
Re: Help on the warning "No objects selected" in ADS2011 schematic environment
Posted: Jul 16, 2012 10:52 AM   in response to: AaronHe in response to: AaronHe
Click to report abuse...   Click to reply to this thread Reply
Aaron,

Please contact Agilent EEsof Technical Support. You can get local phone number and email by visiting http://edocs.soco.agilent.com/display/support/ADS+Support+Home This link also provides access to ADS documentation, training materials, and extensive library of applications and to ask for technical support help.

ADS Product Manager
AaronHe

Posts: 3
Registered: 07/07/12
Re: Help on the warning "No objects selected" in ADS2011 schematic environment
Posted: Jul 17, 2012 3:26 AM   in response to: ADSProductManager in response to: ADSProductManager
Click to report abuse...   Click to reply to this thread Reply
Attachment ADS2011 warning.png (184.7 KB)
Hi Sir:
It seems that I did not describe my question clear at all.
I do not mean that there is something wrong with my ADS 2011 software, I mean that I do not prefer to use the new feature of ADS 2011 and I want to know that is there any method to disable the new feature or not.

In ADS 2011 schematic environment, if you double click mouse's left key or drag a rectangle in the blank area with you mouse, then the warning " No Objects Selected" will come out. There is no warning at all for all the previous ADS version. And I really do not think that this new feature is helpful and all. What's more, sometime it is really annoying. So is there any setting to disable this warning?
The screen capture about this warnning is attached.
Thanks a lot and look forward to the feedback.
eyeung

Posts: 50
Registered: 01/22/09
Re: Help on the warning "No objects selected" in ADS2011 schematic environment
Posted: Jul 20, 2012 11:05 AM   in response to: AaronHe in response to: AaronHe
Click to report abuse...   Click to reply to this thread Reply
Hi Aaron, I am not seeing this issue in ADS 2011.10. When I double click or drag a rectangle on the empty space of a schematic window I did not get any error. Perhaps you are using an earlier version of ADS 2011 that has this issue ?
AaronHe

Posts: 3
Registered: 07/07/12
Re: Help on the warning "No objects selected" in ADS2011 schematic environment
Posted: Jul 21, 2012 7:28 AM   in response to: eyeung in response to: eyeung
Click to report abuse...   Click to reply to this thread Reply
Hi eyeung, my ADS version is 2011.10 as well. Since yo do not have this issue at all, I suppose that there should be some setting to dis-able this warning.
I did contact Agilent FAE, but it seems that he did not have some clue about this either. And I was suggested to call 800 to get some support! ( I will try this next week.)
Although this warning does not impact the at all, it can be improved anyway.

Point your RSS reader here for a feed of the latest messages in all forums