Contact an Expert

Thread: Documenting Vee PCBA test for ISO 9001


Permlink Replies: 2 - Pages: 1 - Last Post: Jun 5, 2012 7:00 PM Last Post By: kurdle Threads: [ Previous | Next ]
kurdle

Posts: 3
Registered: 06/04/12
Documenting Vee PCBA test for ISO 9001
Posted: Jun 4, 2012 4:24 PM
Click to report abuse...   Click to reply to this thread Reply
Is there a good way to document a test procedure that includes what Vee is doing during the test? Say you are controlling an Agilent 34980A as well as a 7014B O'scope and a Keithley 2100 DMM using Vee. Should I be recording on paper what each test involves, what is controlled, what relays are being activated, what the expected outcome should be? Or is there a better formal way of documenting a test? This is for a PCBA test and there are many test points to have data recorded. And by the way, I already dump the data to an Excel spreadsheet. Thanks!
changmeikuan

Posts: 210
Registered: 08/07/09
Re: Documenting Vee PCBA test for ISO 9001
Posted: Jun 4, 2012 7:48 PM   in response to: kurdle in response to: kurdle
Click to report abuse...   Click to reply to this thread Reply
I do documented the keynote. Some people like to use Notepad object from the Display menu. Alternatively, at any VEE object, right click and select Description, we can enter documentation here as well. After finish, there will be a little red triangle on top right of the VEE object. Hoover the mouse over it and the text entered will be displayed. I use these two most of the time.

Maybe others have more idea :)

-mk

Edited by: changmeikuan on Jun 4, 2012 7:49 PM
kurdle

Posts: 3
Registered: 06/04/12
Re: Documenting Vee PCBA test for ISO 9001
Posted: Jun 5, 2012 7:00 PM   in response to: changmeikuan in response to: changmeikuan
Click to report abuse...   Click to reply to this thread Reply
I guess I wasn't clear. I want to document the test process formally as we have to do that for ISO compliance. I have a Word doc with cells that show each test step with a name, units of measure, a spec with tolerance, now I should show an interpretation of what is going on during that part of the test because they aren't going to open up the program and examine every little step I do (since it would be to confusing to the non-Vee programmer). So I want to put in a brief syopsis of what is going on during the test; i.e: Generator outputs a DC level of 2V, relay 5011 closes in 34980A measurement module, voltage inputs ADC at J12 pin 1, query XXX to pcba returns decimal 12000.
Maybe I answered my own question. But I have not seen any automated controlled hardware testing documentation on the web. All I see is documents for software testing so hence my question.

Point your RSS reader here for a feed of the latest messages in all forums