Contact an Expert

Thread: Reading voltage with no connection at relay


Permlink Replies: 1 - Pages: 1 - Last Post: May 28, 2012 1:32 AM Last Post By: afdzalnazri Threads: [ Previous | Next ]
afdzalnazri

Posts: 8
Registered: 02/09/12
Reading voltage with no connection at relay
Posted: May 27, 2012 9:45 PM
Click to report abuse...   Click to reply to this thread Reply
Hi everyone.

I am using 34970A data acquisition with 34901A 20 channel multiplexer.

I have done the remote command using C# to get the data/value.

Question:

How do I get the voltage value remotely using C# without getting error when there is no connection to the relay inside the multiplexer?

How do I tell the system to return 0V and not reading error when there is no connection to the relay inside the multiplexer?
afdzalnazri

Posts: 8
Registered: 02/09/12
Re: Reading voltage with no connection at relay
Posted: May 28, 2012 1:32 AM   in response to: afdzalnazri in response to: afdzalnazri
Click to report abuse...   Click to reply to this thread Reply
DONE! I just need to make a delay at the C# code else an error will be return, not the value

Point your RSS reader here for a feed of the latest messages in all forums