Contact an Expert

Thread: EEPROM back up disk Verification


Permlink Replies: 2 - Pages: 1 - Last Post: May 25, 2012 6:05 AM Last Post By: SOLT_guy
SOLT_guy

Posts: 268
Registered: 05/30/09
EEPROM back up disk Verification
Posted: Apr 28, 2012 10:20 PM
Click to report abuse...   Click to reply to this thread Reply
Dear Sir:

When I bought my network analyzer (8753C) an EEPROM back up disk (floppy disk) was shipped with my network analyzer.

When I attempt to look at the disk in a Windows O/S based environment, Windows cannot read the disk. It can't even tell me what files are on the disk. Windows keeps requesting that I format the disk.

I am hoping that my disk is not damaged or corrupted.

Since the disk is very old - this NA was in its "heyday" before the desktop PC became an integretated unit (HP sold separate disk drives, HP9122, for its computers), I am hoping that the reason why I can't read from the disk is because the file format may be incompatible with the Windows environment.

Can you tell me the file types that are on a typical EEPROM disk (*.LIF ? or other) and can Windows actually read the filenames that are on the disk (I realize that this question may appear to be simple to answer for a person who has had prior access to many NA EEPROM floppy disks but I can't read from my disk, therefore, I have no way of being certain what file types are on the disk and I don't have access to various NA EEPROM floppy disks).

Also, can you tell me if there is a way I can determine if the disk is good without having to go out and buy an old disk drive?

I have access to a 8753D NA which has a built in disk drive. Can I use this disk drive to determine if my disk is still good? If the answer is yes, can you tell me some of the filenames that I will see on the disk, if the 8753D can read from the 8753C EEPROM disk (this is just a check so that I know that everything is OK with this method)?

Thank you for your past replies and I look forward to reading your next reply.

Edited by: SOLT_guy on Apr 28, 2012 10:21 PM

Edited by: SOLT_guy on Apr 29, 2012 1:01 PM

Edited by: SOLT_guy on Apr 29, 2012 1:07 PM
jvall

Posts: 520
Registered: 12/08/05
Re: EEPROM back up disk Verification
Posted: May 13, 2012 12:52 PM   in response to: SOLT_guy in response to: SOLT_guy
Click to report abuse...   Click to reply to this thread Reply
This is almost certainly a LIF formatted disc. There were routines to read this on a PC using a LIF-to-DOS utility, but I think you needed Win98 or earlier to use it. I do not know what else is out there now.
Some instruments could read both formats...such as the 8711 family...but I am not sure which versions...probably the C versions.
SOLT_guy

Posts: 268
Registered: 05/30/09
Re: EEPROM back up disk Verification
Posted: May 25, 2012 6:05 AM   in response to: jvall in response to: jvall
Click to report abuse...   Click to reply to this thread Reply
Dear JVALL;

Thank you for your feedback. I guess this closes out the discussion unless someone else has something else to add.

I appreciate your information.

Thank you, again.

Point your RSS reader here for a feed of the latest messages in all forums