Contact an Expert

Thread: No interface detected


Permlink Replies: 1 - Pages: 1 - Last Post: Apr 24, 2012 9:29 PM Last Post By: changmeikuan Threads: [ Previous | Next ]
omar.mh

Posts: 4
Registered: 04/23/12
No interface detected
Posted: Apr 24, 2012 1:28 AM
Click to report abuse...   Click to reply to this thread Reply
Hello,
I cannot detect a 4338B milliohmmeter by the Instrument Manager in VEE Pro, but the instrument can be detected using Agilent IO Control, the Agilent Libraries Suite are already updated. I'd really appreciate if someone can help with this issue!!
changmeikuan

Posts: 210
Registered: 08/07/09
Re: No interface detected
Posted: Apr 24, 2012 9:29 PM   in response to: omar.mh in response to: omar.mh
Click to report abuse...   Click to reply to this thread Reply
Do you have other VISA installed i.e. NI VISA? If you have other VISA installed, which VISA is primary?
If restarting VEE doesn't show the instrument, maybe can try to add the instrument manually and key in the VISA address shown in Agilent Connection Expert. After that, try Write/Read simple operation e.g. *IDN? see if it works.

Hope this helps,
-mk

Point your RSS reader here for a feed of the latest messages in all forums