Contact an Expert

Thread: N7700A - Photonic Application Suite Error


Permlink Replies: 2 - Pages: 1 - Last Post: Apr 19, 2012 2:34 AM Last Post By: mkelly Threads: [ Previous | Next ]
Berto74

Posts: 2
Registered: 04/18/12
N7700A - Photonic Application Suite Error
Posted: Apr 18, 2012 2:18 PM
Click to report abuse...   Click to reply to this thread Reply
I get the following error when using the IL Engine:
Driver Error: -1074003958x
Parameter 10 is invalid

What does 'Prameter 10' refrer to?
Berto74

Posts: 2
Registered: 04/18/12
Re: N7700A - Photonic Application Suite Error
Posted: Apr 18, 2012 5:33 PM   in response to: Berto74 in response to: Berto74
Click to report abuse...   Click to reply to this thread Reply
Resolved. Changed the wavelength step to 5 pm and that seemed to fix it.
mkelly

Posts: 178
Registered: 02/06/07
Re: N7700A - Photonic Application Suite Error
Posted: Apr 19, 2012 2:34 AM   in response to: Berto74 in response to: Berto74
Click to report abuse...   Click to reply to this thread Reply
Great, that you got past this quickly.

Regarding the mysterious error message: this is being passed from the 816x Plug&Play driver used by the IL engine.
In this case the command is for setting up the scan, prepare_mflambdascan. The details of these commands are in the help file installed with the driver.

The full command is
hp816x_prepareMfLambdaScan(ViSession ihandle, ViInt32 powerUnit, ViReal64 power, ViInt32 opticalOutput, ViInt32 numberofScans, ViInt32 PWMChannels, ViReal64 startWavelength, ViReal64 stopWavelength, ViReal64 stepSize, ViUInt32 numberofDatapoints, ViUInt32 numberofChannels);

So the 10th parameter is the returned number of data points, calculated from the start, stop and step wavelength parameters. Possibly the chosen values of these gave a larger number of points than supported by the power meter. Many sensor modules are limited to 20k points, while the 81636B and N7745A power meters support up to 100k samples in this application.

Point your RSS reader here for a feed of the latest messages in all forums