Contact an Expert

Thread: 8902A Tuned RF-level test


Permlink Replies: 2 - Pages: 1 - Last Post: Mar 29, 2012 2:37 PM Last Post By: bar28 Threads: [ Previous | Next ]
bar28

Posts: 95
Registered: 09/19/08
8902A Tuned RF-level test
Posted: Mar 27, 2012 5:21 AM
Click to report abuse...   Click to reply to this thread Reply
What is the reason, why 8902A Tuned-RF level performance test using 30MHz
test frequency and not 50MHz? We have also N5531S system and there same
test using 50MHz. Does it couse a big measurement error if 8902A Tuned-RF
level test will be run also at 50MHz?

Edited by: bar28 on Mar 27, 2012 5:41 AM
djwservice

Posts: 1
Registered: 03/27/12
Re: 8902A Tuned RF-level test
Posted: Mar 27, 2012 12:59 PM   in response to: bar28 in response to: bar28
Click to report abuse...   Click to reply to this thread Reply
I believe that this is a traditional frequency for reference attenuators that were calibrated using the IF substitution method that is being used to test or verify the specification of the reference steps in the 8902A.

I suspect that you can use any other frequency as it is converted to the 8902A IF frequency and you are then comparing the 8902IF reported step to the reference expected step.

The whole process is assuming the liniarity of teh 1st mixer and the frequency of test should not matter, as long as you have the actual calibration steps at the test frequency.
Hope this helps.
bar28

Posts: 95
Registered: 09/19/08
Re: 8902A Tuned RF-level test
Posted: Mar 29, 2012 2:37 PM   in response to: djwservice in response to: djwservice
Click to report abuse...   Click to reply to this thread Reply
Thanks a lot. Actualy i thought totally same way. Step attenautor is calibrated in 50MHz. I have already tested to run 8902A Tuned RF-level test using 50MHz and it works perfectly. Using repeatable step attanuator i can monitor our cal lab's 8902A, N5531S and 8510C VNA's levelig accuracy together....50MHz fits also to 8510C's frequency range :-)

Point your RSS reader here for a feed of the latest messages in all forums