Contact an Expert

Thread: Can the multi-tone feature in ESG be used to do two-tone tests?


Permlink Replies: 1 - Pages: 1 - Last Post: Mar 16, 2012 12:07 PM Last Post By: tabbott
tabbott


Posts: 1,483
Registered: 07/24/09
Can the multi-tone feature in ESG be used to do two-tone tests?
Posted: Mar 16, 2012 11:55 AM
Click to report abuse...   Click to reply to this thread Reply
During the Signal Generator Back-to-Basics Webcast, hosted by Agilent Technologies, on 29 February 2012, we received a number of real-time questions from a broad audience.

If one person asks - someone else will want to know the answer too - so we have captured various questions and answers and are posting them individually here, in this Forum, for your future reference and immediate enjoyment!

Question: Could you talk a little bit about the multi-tone feature available in your ESG's? Can we use that to do two-tone tests? What are the limitations?
tabbott


Posts: 1,483
Registered: 07/24/09
Re: Can the multi-tone feature in ESG be used to do two-tone tests?
Posted: Mar 16, 2012 12:07 PM   in response to: tabbott in response to: tabbott
Click to report abuse...   Click to reply to this thread Reply
Answer: An E4438C ESG signal generator equipped with an option 601 or 602 baseband generator can generate multiple tones – from 2 to 64, with selectable on/off state per tone. The tones must all fit within an 80 MHz bandwidth centered about the carrier frequency. This capability can provide a convenient space-saving and cost-effective alternative to combining the outputs of multiple analog signal generators. These same multi-tone capabilities are also available in the N5182A MXG and E8267D PSG vector signal generators.
If more tones are needed, you can use any of these signal generators in conjunction with the N7621B Signal Studio for Multi-tone Distortion software (see: http://www.home.agilent.com/agilent/product.jspx?cc=US&lc=eng&pageMode=OV&pid=1160743&ct=PRODUCT&id=1160743). This setup enables you to generate up to 4097 tones within the 80 MHz bandwidth and provides a pre-distortion algorithm to correct the signals, greatly improving the distortion-free dynamic range.

Point your RSS reader here for a feed of the latest messages in all forums