Contact an Expert

Discussion Forums are temporarily in read only mode. All forums are visible but posting is not possible. Please check back shortly.

Thread: 53220A LXI Comms Intermittent


Permlink Replies: 0 - Pages: 1 Threads: [ Previous | Next ]
mark.fons@plexu...

Posts: 1
Registered: 12/14/11
53220A LXI Comms Intermittent
Posted: Dec 14, 2011 2:42 PM
Click to report abuse...   Click to reply to this thread Reply
We are occasionally having problems communicating with our new 53220A's. We have 5 systems all with one of these instruments, and it is the only instrument giving us any problems. Details:
1) We are using LXI, fixed IP address
2) It is a closed network, only with Agilent equipment
3) The unit's webpage works flawlessly (no issues seen when using instrument "interactively")
4) We occasionally have to retry comms commands, like TVISADEVICE OPEN, or other commands like setting up instrument
5) We do not see errors on the instrument, the problem shows itself like the comms commands are simply missed
6) We have had to retry 2-4 times, but retrying always seems to works

Point your RSS reader here for a feed of the latest messages in all forums