Contact an Expert

Thread: difficulty to change stability in agilent counter 35132


Permlink Replies: 5 - Pages: 1 - Last Post: Jan 13, 2012 12:38 PM Last Post By: lhornburg Threads: [ Previous | Next ]
walid

Posts: 16
Registered: 12/16/11
difficulty to change stability in agilent counter 35132
Posted: Jan 11, 2012 3:29 AM
Click to report abuse...   Click to reply to this thread Reply
HI all
please how i can change the stability in my counter 35132 A from 001 MS oven to 012 US oven ,manually and automatic(wish commands i can use);

thanks
weicher

Posts: 6
Registered: 01/10/12
Re: difficulty to change stability in agilent counter 35132
Posted: Jan 11, 2012 5:03 AM   in response to: walid in response to: walid
Click to report abuse...   Click to reply to this thread Reply
Hi walid,

as far as I know these are options which you must buy from agilent.
These options replace the internal reference oscillator, so you may have only one option installed either option 001 or 010 or 012.

SENS:ROSC:SOUR knows only INT or EXT

best regards
Walter
walid

Posts: 16
Registered: 12/16/11
Re: difficulty to change stability in agilent counter 35132
Posted: Jan 11, 2012 6:48 AM   in response to: walid in response to: walid
Click to report abuse...   Click to reply to this thread Reply
thanks weicher ,please if i change sensitivity ,this sensibility option can change ????
weicher

Posts: 6
Registered: 01/10/12
Re: difficulty to change stability in agilent counter 35132
Posted: Jan 12, 2012 2:04 AM   in response to: walid in response to: walid
Click to report abuse...   Click to reply to this thread Reply
Hi walid,

"
please if i change sensitivity ,this sensibility option can change ????
"


I dont no exactly what you mean...
But I think NO because these options are hardware parts.

If these hardware parts are missing on your counter, then you can not activate them by software.

Best regards
Walter
walid

Posts: 16
Registered: 12/16/11
Re: difficulty to change stability in agilent counter 35132
Posted: Jan 12, 2012 7:09 AM   in response to: walid in response to: walid
Click to report abuse...   Click to reply to this thread Reply
hi
thanks for help

Best regards
lhornburg

Posts: 492
Registered: 01/15/10
Re: difficulty to change stability in agilent counter 35132
Posted: Jan 13, 2012 12:38 PM   in response to: walid in response to: walid
Click to report abuse...   Click to reply to this thread Reply
Only one timebase option can be installed the 53131A (Option 001, Option 010, or Option 012).

The Option 012 timebase for the 53131A counter is customer installable. In order for the instrument to be retrofitted with Option 012 the instrument must have firmware revision 3402 or greater. To determine the firmware revision turn the instrument off, press and hold the RECALL key, and press the POWER button to turn the instrument on. The revision number will appear in the display.

The parts required for the retrofit include:

quantity 1 A6 Timebase Support Board 53132-60016
quantity 1 Oven Oscillator 10811-60260
quantity 3 TORX 10 Screws (H2) 0515-0430
quantity 2 Pozidriv Screws (H7) 2360-0331

These parts are available from Agilent and are purchased individually. Installation instructions can be found beginning on page 4-11 of the Assembly-Level Service Guide found online at http://cp.literature.agilent.com/litweb/pdf/53131-90039.pdf.

Point your RSS reader here for a feed of the latest messages in all forums