Contact an Expert

Thread: 8257D Step/List Sweep external Trigger


Permlink Replies: 1 - Pages: 1 - Last Post: Nov 23, 2011 2:38 PM Last Post By: tabbott Threads: [ Previous | Next ]
BrianR

Posts: 6
Registered: 03/09/06
8257D Step/List Sweep external Trigger
Posted: Nov 23, 2011 12:09 PM
Click to report abuse...   Click to reply to this thread Reply
Is it possible to step thru the frequency list in List or Step mode using an external trigger instead of specifying the dwell time? From what I can tell, it looks like the external trigger only initiates the list sequence.
tabbott


Posts: 1,483
Registered: 07/24/09
Re: 8257D Step/List Sweep external Trigger
Posted: Nov 23, 2011 2:38 PM   in response to: BrianR in response to: BrianR
Click to report abuse...   Click to reply to this thread Reply
Hi -

Yes, it is possible to step thru the sweep elements (frequency and/or amplitude) in either List or Step mode.

After setting up the desired Sweep elements configure as follows:
Set Sweep Repeat to ‘Cont’
Set Sweep Trigger to ‘Free Run’
Set Point Trigger to ‘Ext’
Turn the sweep ‘On’

Now each single external trigger will cause a transition to the next sweep element.

Regards -

Point your RSS reader here for a feed of the latest messages in all forums