Contact an Expert

Thread: Defect of "goldenGateLib/YF"


Permlink Replies: 0 - Pages: 1
TNAKA

Posts: 83
Registered: 06/08/09
Defect of "goldenGateLib/YF"
Posted: Nov 22, 2009 3:48 AM
Click to report abuse...   Click to reply to this thread Reply
I have question about "goldenGateLib/YF".

If we choose "TYPE=2", "goldenGateLib/YF" is gamma(rho/phi) setting mode.
But there is no parameter for setting reference impedance.

Reference impedance is not treated as 50Ohm.
It seems "re" parameters for "impedance (re/imag)(TYPE=1)" setting mode is used as reference impedance value.

Why does not "goldenGateLib/YF" have z0, reference impedance parameter ?
Why does "goldenGateLib/YF" treat "re" parameters for "impedance (re/imag)(TYPE=1)" setting mode as reference impedance value ?
Why don't you arrange setting parameters of "goldenGateLib/YF" completely as same as "goldenGateLib/ZF" ?

We can't substitute YF with ZF.

Point your RSS reader here for a feed of the latest messages in all forums