Contact an Expert

Thread: Layout unit in ADS 2011.05


Permlink Replies: 1 - Pages: 1 - Last Post: Dec 23, 2011 11:32 AM Last Post By: sdgrant
vanhoang_nguyen

Posts: 3
Registered: 03/24/10
Layout unit in ADS 2011.05
Posted: Dec 14, 2011 8:31 AM
Click to report abuse...   Click to reply to this thread Reply
Hello,

We recently have ADS 2011.05 installed. When working with Layout, I notice that the Layout unit tab (Options --> Preferences --> Preferences for Layout) is no longer available in this version while it was previously available in ADS 2009, update 1. I have the following question:

- Is there an option in ADS 2011.05 to change/set my Layout unit (for example, layout unit is always in inch)?

Thank you,

Hoang
sdgrant


Posts: 120
Registered: 06/08/09
Re: Layout unit in ADS 2011.05
Posted: Dec 23, 2011 11:32 AM   in response to: vanhoang_nguyen in response to: vanhoang_nguyen
Click to report abuse...   Click to reply to this thread Reply
The units are set in the library that is being used to save the designs. In the Main window select Options > Technology > Technology Setup...

The Layout Units tab is when both the Units and the Resolution are set.

Point your RSS reader here for a feed of the latest messages in all forums