Contact an Expert

Thread: Report window buffer limited


Permlink Replies: 1 - Pages: 1 - Last Post: Apr 15, 2010 3:51 AM Last Post By: jszlatki Threads: [ Previous | Next ]
ses

Posts: 1
Registered: 11/23/09
Report window buffer limited
Posted: Apr 13, 2010 1:26 AM
Click to report abuse...   Click to reply to this thread Reply
Hi all,
I'm using TestExec 4.1 and notice that long outputs in the report window are cutted after appr. 800 lines or 40kB size.
Does someone know if and how I can increase the report window buffer?

Thanks in advance,
Sebastian
jszlatki

Posts: 14
Registered: 08/18/09
Re: Report window buffer limited
Posted: Apr 15, 2010 3:51 AM   in response to: ses in response to: ses
Click to report abuse...   Click to reply to this thread Reply
Hi Sebastian,

I use TE6.1 (and earlier 5.1). So I'm not sure if this works at TE4.1.
So the solution is in the Preferences.upf file.

Report Window
; Specifies the text buffer size (in kilobytes) of the Report Window. Integer
; values between 1 - 1023 are valid; the default is 64. To conserve memory, it
; is recommended that the value be set just slightly higher than the required
; report text size.
Text Buffer Size =512

regards,
Joey

Point your RSS reader here for a feed of the latest messages in all forums