Contact an Expert

Thread: LCA N4373C


Permlink Replies: 2 - Pages: 1 - Last Post: Jan 23, 2012 8:39 PM Last Post By: motoman89 Threads: [ Previous | Next ]
motoman89

Posts: 14
Registered: 07/11/11
LCA N4373C
Posted: Jan 23, 2012 2:30 AM
Click to report abuse...   Click to reply to this thread Reply
Hello!
I would like to clarify the following situation:
The analyzer of optical components N4373 consists of two parts: the vector network analyzer and an optical measuring unit N4373-101. Production of these components occurs are separately. How does the calibration of these components: separately or only as part of the analyzer N4373C? Is there a technical possibility to calibrate the modules separately?
mkelly

Posts: 178
Registered: 02/06/07
Re: LCA N4373C
Posted: Jan 23, 2012 5:15 AM   in response to: motoman89 in response to: motoman89
Click to report abuse...   Click to reply to this thread Reply
Hello motoman89,
Like you say, the N4373C and other LCA models does include a network analyzer that has its own complete calibration. This instrument is then included in the production and calibration of the N4373C that incorporates the electro-optical instrumentation. So there is not an independent calibration procedure for the optical measurement unit and the specifications are achieved by calibration as an integrated unit.
Best regards,
Mike
motoman89

Posts: 14
Registered: 07/11/11
Re: LCA N4373C
Posted: Jan 23, 2012 8:39 PM   in response to: motoman89 in response to: motoman89
Click to report abuse...   Click to reply to this thread Reply
Thank you!

Point your RSS reader here for a feed of the latest messages in all forums