Contact an Expert

Thread: HP3458A err message


Permlink Replies: 3 - Pages: 1 - Last Post: Oct 10, 2011 2:35 PM Last Post By: lhornburg
Robbie

Posts: 2
Registered: 10/04/11
HP3458A err message
Posted: Oct 4, 2011 10:44 AM
Click to report abuse...   Click to reply to this thread Reply
Can anyone tell me what "err" means (other than the obvious!). I get it when either turning on HP3458A or when doing a "test" function from the front panel. The "err" message appears when it finishes doing ROM and RAM tests and when it starts the "Slave test".
I have two 3458A's one says "self test failed" when it gives up; the other fails to a "VDC" state.

If it is beyond the user to fix can you tell me where I need to send them to get fixed, please.

Thanks
lhornburg

Posts: 493
Registered: 01/15/10
Re: HP3458A err message
Posted: Oct 6, 2011 11:21 AM   in response to: Robbie in response to: Robbie
Click to report abuse...   Click to reply to this thread Reply
Yes you are correct, it means exactly what you think it does, there is an error. Now you need to read the error message by checking it on the front panel so we know what were dealing with. See page 31 of the user's guide for instructions on how to check the error messages then please reply with the messages so we can help you out.Image
Robbie

Posts: 2
Registered: 10/04/11
Re: HP3458A err message
Posted: Oct 10, 2011 10:17 AM   in response to: Robbie in response to: Robbie
Click to report abuse...   Click to reply to this thread Reply
202 hardware failure slave test AC board
and fails to V DC

Thanks
lhornburg

Posts: 493
Registered: 01/15/10
Re: HP3458A err message
Posted: Oct 10, 2011 2:35 PM   in response to: Robbie in response to: Robbie
Click to report abuse...   Click to reply to this thread Reply
Hello Robbie,

Unfortunately this means there is probably an issue with A2 board, which is the AC converter assembly. I would suggest sending it in to an Agilent service center for repair. The USA contact number is

toll-free:
+1 800 829-4444 Press #, then 3

Point your RSS reader here for a feed of the latest messages in all forums