Contact an Expert

Discussion Forums are temporarily in read only mode. All forums are visible but posting is not possible. Please check back shortly.

Thread: Signal Studio Toolkit


Permlink Replies: 1 - Pages: 1 - Last Post: Sep 27, 2011 2:21 PM Last Post By: tabbott Threads: [ Previous | Next ]
andpas

Posts: 1
Registered: 09/20/11
Signal Studio Toolkit
Posted: Sep 20, 2011 3:40 AM
Click to report abuse...   Click to reply to this thread Reply
Hello.
We have a ESG generator with IQ generation option.
I'm trying to upload IQ data files to the instrument using Signal Studio Toolkit.
When I try to connect to the instrument, the system succesfully initiate communication with GPIB, but after I press the button "FINISH" to finalize instrument configuration, something goes wrong, telling that intrument cannot be used.
I don't underdstand if it depends on instrument configuration, missing hardware/software options enabled, firmware bugs or whatever...
Please, could you clarify what are the minimum requirements on the instrument side to use the software?
Thanks
tabbott


Posts: 1,483
Registered: 07/24/09
Re: Signal Studio Toolkit
Posted: Sep 27, 2011 2:21 PM   in response to: andpas in response to: andpas
Click to report abuse...   Click to reply to this thread Reply
Hi -

The minimum Hardware requirement for the ESG when used with the N7622A Signal Studio Toolkit:
Model Number – E4438C
Firmware revision – C.04.10 or later
Option 601 or 602 installed.

Regards -

Point your RSS reader here for a feed of the latest messages in all forums