Contact an Expert

Thread: what is device modelling?


Permlink Replies: 1 - Pages: 1 - Last Post: Jun 16, 2010 10:26 AM Last Post By: bharatindana
guruja

Posts: 1
Registered: 04/15/10
what is device modelling?
Posted: Apr 15, 2010 3:11 PM
Click to report abuse...   Click to reply to this thread Reply
What is the need of Device modelling?Example:ebber moll model.
What impact does it have on Analog design?
bharatindana

Posts: 2
Registered: 12/14/09
Re: what is device modelling?
Posted: Jun 16, 2010 10:26 AM   in response to: guruja in response to: guruja
Click to report abuse...   Click to reply to this thread Reply
In an analog circuit simulation to calculate the voltage/current at any node, simulator requires information about electrical characteristics of each device.
This is provided in the form of a set of equations and parameters to the simulator.
set of equations used to describe the device characteristics is called model eg: BSIM3
parameters are the variables input to these equations so that the device characteristics from simulation are same as observed in actual measurement for a particular device.
eg., of parameters: threshold voltage, mobility.
Determining these parameters for a particular device to match simulation and measurement is called parameter extraction.
I have a mos fabraicated in silicon. I have some measured data for particular vgs and vds.
I use the measurement data and model and extract parameters so that the simulated result is same as measured data.
Then using this model I can simulate the device for any vgs and vds and know the output current.
This is the need of device modeling.
Proper model implies it reflects the fabrication technology exactly.

Point your RSS reader here for a feed of the latest messages in all forums