Contact an Expert

Thread: S parameter impedance conversion


Permlink Replies: 2 - Pages: 1 - Last Post: Apr 25, 2011 1:50 PM Last Post By: Trevor.Bartram Threads: [ Previous | Next ]
Trevor.Bartram

Posts: 8
Registered: 04/22/11
S parameter impedance conversion
Posted: Apr 22, 2011 8:18 AM
Click to report abuse...   Click to reply to this thread Reply
I am new to Genesys, I havn't used it yet but when I do, one of the first things I'll have to do involves taking published s parameter device files and converting them from 50 Ohm system impedance to 75 Ohm, as I'm working in the cable TV industry.
I have used Touchstone and MW Office extensively in the past but never with a system impedance other than 50 Ohm. Does Genesys have the capability to automatically convert the impedance of s parameter files?
Thanks, Trevor.
RANDY_RHEA

Posts: 351
Registered: 06/08/09
Re: S parameter impedance conversion
Posted: Apr 25, 2011 1:43 PM   in response to: Trevor.Bartram in response to: Trevor.Bartram
Click to report abuse...   Click to reply to this thread Reply
Hello Trevor,

GENESYS is automatic. You don't need to do anything. Load the 50-ohm S-parameter file and just specify 75 ohm ports in your schematic.

If you need a converted S-parameter data file for another application, create a simple schematic with two 75 ohm ports connected to the two-port and export the data. The exported file will be the converted S-parameter data with 75 ohms specified in the file header.

Clear skies and high Q
Trevor.Bartram

Posts: 8
Registered: 04/22/11
Re: S parameter impedance conversion
Posted: Apr 25, 2011 1:50 PM   in response to: Trevor.Bartram in response to: Trevor.Bartram
Click to report abuse...   Click to reply to this thread Reply
Hi Randy,
Understood. Thanks.
Trevor.

Point your RSS reader here for a feed of the latest messages in all forums