Contact an Expert

Thread: OscTest


Permlink Replies: 1 - Pages: 1 - Last Post: Apr 19, 2010 11:07 AM Last Post By: RANDY_RHEA Threads: [ Previous | Next ]
rfehn

Posts: 25
Registered: 06/08/09
OscTest
Posted: Apr 16, 2010 6:19 AM
Click to report abuse...   Click to reply to this thread Reply
Hello

It would be nice to have an OscTest port to simulate the small-signal loop gain of the oscillator.

Roy
RANDY_RHEA

Posts: 351
Registered: 06/08/09
Re: OscTest
Posted: Apr 19, 2010 11:07 AM   in response to: rfehn in response to: rfehn
Click to report abuse...   Click to reply to this thread Reply
Attachment Template.wsx (684.7 KB)
Hello Roy,

You are absolutely correct. Simulating the open-loop, small-signal transfer and reflection characteristics is critical to understanding oscillator behavior. If the designer only simulates the closed-loop circuit in the oscillation mode, they do not know the gain margin, or if maximum phase slope occurs at the gain peak, or if improved matching could increase the gain margin, or if multiple phase zero crossings occur. In fact, they know little more than with the final constructed oscillator. Yes, it oscillates, but what is the design quality.

The Oscport feature in GENESYS automatically provides the steady-state excitation signal for an HB analysis and unloads that source from the oscillator. But it does not simulate the open-loop, small-signal characteristics. As you suggest, the Oscport feature could be expanded to include two-ports for the open-loop characteristics. However, some type of interface would be required for the user to specify which side (left or right) of the port is the input and which is the output.

For use until such an enhancement is added, an oscillator simulation workspace is attached in this post. This "template.wsx" workspace includes an open-loop, small-signal simulation schematic along with a reuse of that schematic in a closed loop oscillator simulation. I use this template to begin all of my oscillator designs. All I have to do is replace the open-loop schematic with my design. The template workspace includes all the setups for the open-loop analysis, closed-loop HB analysis, a Cayenne time-step simualtion for starting, nonlinear HB noise analysis, and appropriate output graphs. It saves a lot of time. I hope you find it helpful. In a month or two, Agilent will be adding a site to download some 70 or so oscillator workspaces I used while writing the new oscillator book.

Clear skies and high Q

Point your RSS reader here for a feed of the latest messages in all forums