Contact an Expert

Thread: API function to get Description of Data


Permlink Replies: 2 - Pages: 1 - Last Post: Dec 10, 2011 12:34 PM Last Post By: ses72
ses72

Posts: 3
Registered: 06/21/11
API function to get Description of Data
Posted: Aug 25, 2011 5:40 AM
Click to report abuse...   Click to reply to this thread Reply
Attachment x.jpg (45.0 KB)
Attachment y.jpg (13.1 KB)
Hi,

I'm looking for a function to programatically retrieve the description of action parameters (see pictures).
Currently I'm using .NET to talk with TestExec but there seams no appropriate function for this in the Data class. Is there may be a C interface dll I can use?
Image Image

Thanks in advance,
Sebastian
OnlyOne

Posts: 110
Registered: 07/26/07
Re: API function to get Description of Data
Posted: Nov 22, 2011 1:54 AM   in response to: ses72 in response to: ses72
Click to report abuse...   Click to reply to this thread Reply
When you try to retrieve the information from a loaded testplan then you can perhaps use the View+Listing-functions (if they are available in .Net).
Best regards
ses72

Posts: 3
Registered: 06/21/11
Re: API function to get Description of Data
Posted: Dec 10, 2011 12:34 PM   in response to: ses72 in response to: ses72
Click to report abuse...   Click to reply to this thread Reply
thanks for the reply.
These functions are not available in the .NET interfaces. But I found a way. "Simply" use the dll functions from utacore.dll and pubapi.dll

Regards,
Sebastian

Point your RSS reader here for a feed of the latest messages in all forums