Contact an Expert

Thread: LA 16900 Programmer Manual


Permlink Replies: 1 - Pages: 1 - Last Post: May 13, 2011 10:15 AM Last Post By: algoss
fada

Posts: 5
Registered: 01/18/10
LA 16900 Programmer Manual
Posted: May 13, 2011 12:22 AM
Click to report abuse...   Click to reply to this thread Reply
Hi,

I want to use LA 16902A remotely by using c#. but I could not find programmer manual someone can help me about this. In addition to this, I use visa com to communicate with spectrum analyzer , network analyzer, etc. is it possible for LA 16902A?
algoss


Posts: 637
Registered: 11/03/06
Re: LA 16900 Programmer Manual
Posted: May 13, 2011 10:15 AM   in response to: fada in response to: fada
Click to report abuse...   Click to reply to this thread Reply
There is no separate manual for 16900 programming. Everything is in the help file, which is loaded with the software, or can be gotten as a separate download from the Agilent website. Use the index to get to 'COM Automation'.

Programming is done through a Windows COM or DCOM connection, so there is not a visa driver, as far as I know. This is VERY different from the SCPI commands that are used for other instruments.

There are example programs provided through the menu. Start -> Programs -> Agilent Logic Analyzer -> Utilities -> COM Automation. The source for some additional languages, including Python, Perl, and Tcl, is in the help file.

Algoss

Point your RSS reader here for a feed of the latest messages in all forums