Contact an Expert

Thread: C# programming to connect to 16804A Logic Analyzer


Permlink Replies: 2 - Pages: 1 - Last Post: Mar 31, 2011 6:12 AM Last Post By: algoss
khung

Posts: 2
Registered: 03/25/11
C# programming to connect to 16804A Logic Analyzer
Posted: Mar 25, 2011 1:24 PM
Click to report abuse...   Click to reply to this thread Reply
Is there any C# sample code that illustrates how to communicate with the Instrument COM Automation Server to connect to the 16804A Logic Analyzer hardware from a remote computer (via Ethernet network) and starts measurement. I found examples in VBscript, C++, Python, TCL, Perl but not C#.
khung

Posts: 2
Registered: 03/25/11
Re: C# programming to connect to 16804A Logic Analyzer
Posted: Mar 25, 2011 1:49 PM   in response to: khung in response to: khung
Click to report abuse...   Click to reply to this thread Reply
By the way, I included the Agilent agClientSvr.dll as the API in my Visual C# environment to try to connect to the logic analyzer. Don't know if this is the correct one to use.
algoss


Posts: 641
Registered: 11/03/06
Re: C# programming to connect to 16804A Logic Analyzer
Posted: Mar 31, 2011 6:12 AM   in response to: khung in response to: khung
Click to report abuse...   Click to reply to this thread Reply
There are no C# examples, as far as I know. I know that some customers have used C# successfully to connect to the analyzers, and that some of my colleagues have written code as part of consulting contracts. Neither of those is available in a free form.

AG

Point your RSS reader here for a feed of the latest messages in all forums