Contact an Expert

Thread: Paging a Dual SIM phone using 2 8960's


Permlink Replies: 1 - Pages: 1 - Last Post: May 20, 2011 4:31 PM Last Post By: tabbott Threads: [ Previous | Next ]
muchakra

Posts: 3
Registered: 04/06/11
Paging a Dual SIM phone using 2 8960's
Posted: May 5, 2011 10:24 AM
Click to report abuse...   Click to reply to this thread Reply
Hi

I have one test case scenario at on of my customers site:

The use case is just making MT call on one of the SIMs/ both the SIMs simultaneously and take the statistics ( Like How many calls passed & Not established)

But.... The precondition for this is “ Both the SIMs PCH/PPCH logical channels should get overlap
This is what is required to be created using 8960

Objective : In Dual Sim Dual Standby Phone, we will have on RF baseband and two SIMS to server basically receive data from both the networks
So..... if the paging channels overlap then it will be difficult to receive both of them at the same time and we want to measure how efficient the RF driver is to receive and decode both the page.

Do let me know incase any one has tried this scenario.

Thanks
Chaitanya
tabbott


Posts: 1,483
Registered: 07/24/09
Re: Paging a Dual SIM phone using 2 8960's
Posted: May 20, 2011 4:31 PM   in response to: muchakra in response to: muchakra
Click to report abuse...   Click to reply to this thread Reply
Hi -

I really doubt we can sync up two 8960 to page at the same time.
It seems in your request, the two 8960 must page the mobile phone at the same time, or at the paging group, but it is hard to control two 8960 to send paging at the same time .
We have never done such a experiment before.

Regards -

Point your RSS reader here for a feed of the latest messages in all forums