Contact an Expert

Thread: :MEASure:OVERshoot (how to configure rising/falling edge)


Permlink Replies: 1 - Pages: 1 - Last Post: Jun 22, 2010 5:37 PM Last Post By: dnt Threads: [ Previous | Next ]
JefferyB

Posts: 8
Registered: 05/28/10
:MEASure:OVERshoot (how to configure rising/falling edge)
Posted: May 28, 2010 9:46 AM
Click to report abuse...   Click to reply to this thread Reply
I'm using VBA (Excel) to configure measurements on my DSO80204, using the :MEASure:OVERshoot command sets up the measurement on the scope for rising edge by default. Is there a way to extend the functionality of the command (or all other MEASure commands) to set the detailed parameters such as the thresholds and edge direction on which the measurement is made?

I can set all this up locally on the scope but I'd rather find a way to do this via VBA, I'm just getting into remote programming so maybe I've just missed some details in the programming guide.

Cheers,

Jeff
dnt

Posts: 223
Registered: 02/15/06
Re: :MEASure:OVERshoot (how to configure rising/falling edge
Posted: Jun 22, 2010 5:37 PM   in response to: JefferyB in response to: JefferyB
Click to report abuse...   Click to reply to this thread Reply
Check the :meas:threshold commands and see if they do what you want.

Point your RSS reader here for a feed of the latest messages in all forums