Contact an Expert

Thread: The remote control problem in Agilent 8960


Permlink Replies: 0 - Pages: 1
jerrystone

Posts: 1
Registered: 02/08/12
The remote control problem in Agilent 8960
Posted: Feb 9, 2012 12:11 AM
Click to report abuse...   Click to reply to this thread Reply
Hi,

The problem is when I connect handheld device with 8960 successfully, the state of active cell shows "Attached", but I send GPIB command by LabVIEW to 8960, ex: CALL:BAND EGSM or CALL:BCH 38...etc, the state of active cell will change from "Attached" to "Idle". There is no this issue when I set BCH parameters by manual. Could anyone help me to solve it? thanks!

Jerry

Point your RSS reader here for a feed of the latest messages in all forums