Contact an Expert

Thread: help in 34970A or 34972A


Permlink Replies: 1 - Pages: 1 - Last Post: Aug 6, 2012 11:34 AM Last Post By: mkawasaki
walid

Posts: 16
Registered: 12/16/11
help in 34970A or 34972A
Posted: Aug 6, 2012 9:08 AM
Click to report abuse...   Click to reply to this thread Reply
Hello
Please how i can use the module (34901 and 34903A) ,how i can connect between two test point for example i have 52 voltage measurement how i can doet and how i can play with my modul
mkawasaki

Posts: 72
Registered: 12/12/05
Re: help in 34970A or 34972A
Posted: Aug 6, 2012 11:34 AM   in response to: walid in response to: walid
Click to report abuse...   Click to reply to this thread Reply
walid wrote:
> Hello
Please how i can use the module (34901 and 34903A) ,how i can connect between two test point for example i have 52 voltage measurement how i can doet and how i can play with my modul

I would suggest you post in the Data Acquisition section. This is specifically designed to answer the 34970 questions. http://www.home.agilent.com/owc_discussions/forum.jspa?forumID=128

I could post for you, but better if you post so you can see the answers through email notification.

Hope this helps!

Mike Kawasaki
Agilent

Point your RSS reader here for a feed of the latest messages in all forums