Contact an Expert

Thread: X-Series Signal Analzyers alignment program


Permlink Replies: 1 - Pages: 1 - Last Post: Jul 30, 2012 3:50 PM Last Post By: tabbott
zwm

Posts: 2
Registered: 07/08/12
X-Series Signal Analzyers alignment program
Posted: Jul 8, 2012 8:50 PM
Click to report abuse...   Click to reply to this thread Reply
Agilent has an example program for running alignments and polling to see when they are complete at:
www.agilent.com/find/sa_programming

Unluckily, there is no alignment example for X-Series Signal Analzyers. I think the X-series can be compatible with remote control codes of PSA-series, so I try the alignment example of PSA-series for X-Series. But it give the error: the polling query "*ESR?" timeout. It seems that the execution of "CAL:ALL" blocks all following remote control codes.

Anyone has good solution for the alignment example for X-Series Signal Analzyers?
tabbott


Posts: 1,483
Registered: 07/24/09
Re: X-Series Signal Analzyers alignment program
Posted: Jul 30, 2012 3:50 PM   in response to: zwm in response to: zwm
Click to report abuse...   Click to reply to this thread Reply
Hi -

You will want to perform the CAL:ALL and then serial poll the STB? and look for 32, once you have this you can query the ESR? register.

Regards -

Point your RSS reader here for a feed of the latest messages in all forums