Contact an Expert

Thread: MXA N9020A Calibration Operation Complete Question


Permlink Replies: 1 - Pages: 1 - Last Post: Jul 30, 2012 3:49 PM Last Post By: tabbott Threads: [ Previous | Next ]
Tom003

Posts: 1
Registered: 07/11/12
MXA N9020A Calibration Operation Complete Question
Posted: Jul 11, 2012 7:42 AM
Click to report abuse...   Click to reply to this thread Reply
I am checking the Status:Questionable:Calibration:Condition register.
When the return value is 16384, I know I need to calibrate the unit.
I then issue the command Calibrate:All
No problems so far, everything is working as expected.

The issue is then calling "*OPC?" to determine if the cal process is complete, results in a timeout error.
Why a timeout error? or How do I go about determining when the calibration is complete?

Thanks in advance.

Tom
tabbott


Posts: 1,483
Registered: 07/24/09
Re: MXA N9020A Calibration Operation Complete Question
Posted: Jul 30, 2012 3:49 PM   in response to: Tom003 in response to: Tom003
Click to report abuse...   Click to reply to this thread Reply

Point your RSS reader here for a feed of the latest messages in all forums