Contact an Expert

Thread: PNA E8364A Sweep Average


Permlink Replies: 3 - Pages: 1 - Last Post: Jul 5, 2012 2:02 PM Last Post By: huimingx24
huimingx24

Posts: 3
Registered: 07/30/10
PNA E8364A Sweep Average
Posted: Jun 30, 2012 5:12 PM
Click to report abuse...   Click to reply to this thread Reply
Attachment untitled.bmp (380.2 KB)
Hi Everyone,

I have some problem when I try to use sweep average during S-parameter measurement. I set the sweep average to 10. On the screen, it shows the sweep count correctly. However, when I try to use Vee program to grab the averaged data. It doesn't wait until the whole average is done before giving me the data. However can I let the PNA wait until average is done before return the S-Parameter value? In the attachment is the vee code I wrote to do the S-parameter measurement. Thanks!
Dr_joel


Posts: 2,788
Registered: 12/01/05
Re: PNA E8364A Sweep Average
Posted: Jul 1, 2012 3:08 PM   in response to: huimingx24 in response to: huimingx24
Click to report abuse...   Click to reply to this thread Reply
You need to use the groups control, not init:imm; Init:imm means "take as sweep and return right away". For you , you need to use groups.

Send these commands:
(early in the program)
sens:swe:mode hold !this holds the sweeps and makes programming faster to respond

Trig:sour imm ! this puts the PNA in normal internal triggered mode
SENS:AVER:CLE ! this resets the averaging
sens:aveg:coun 10 ! set this to the number of averages
sens:swe:gro:coun 10 ! set this to the number of averages
sens:swe:mode gro ! take 10 sweeps
opc? ! opc returns when 10 sweeps are finished.

Use this sequence always, (even when not averaging). To do single sweeps, set the count to 1.

huimingx24

Posts: 3
Registered: 07/30/10
Re: PNA E8364A Sweep Average
Posted: Jul 5, 2012 10:21 AM   in response to: Dr_joel in response to: Dr_joel
Click to report abuse...   Click to reply to this thread Reply
Hi Drjoel,

I followed the instructions. However, when I tried to run the program, it gives an error "undefined header". It seems can not recognize "SENS:SWE:MODE GRO". Do you have any idea what might be problem? Thanks!
huimingx24

Posts: 3
Registered: 07/30/10
Re: PNA E8364A Sweep Average
Posted: Jul 5, 2012 2:02 PM   in response to: huimingx24 in response to: huimingx24
Click to report abuse...   Click to reply to this thread Reply
I made a stupid mistake. The problem has been resolved. Thanks!

Point your RSS reader here for a feed of the latest messages in all forums