Contact an Expert

Thread: PNA Measures as function of Angular Frequency or Frequency?


Permlink Replies: 4 - Pages: 1 - Last Post: Jun 28, 2012 12:56 PM Last Post By: Dr_joel Threads: [ Previous | Next ]
jaz

Posts: 25
Registered: 04/17/10
PNA Measures as function of Angular Frequency or Frequency?
Posted: Jun 28, 2012 8:51 AM
Click to report abuse...   Click to reply to this thread Reply
Hello,

I am trying to use measured S parameter data to perform some analysis and calculation. However, i am not sure if PNA measurement is done as a function of frequency or angular frequency. Thank you in advance.

daras


Posts: 920
Registered: 12/01/05
Re: PNA Measures as function of Angular Frequency or Frequency?
Posted: Jun 28, 2012 10:07 AM   in response to: jaz in response to: jaz
Click to report abuse...   Click to reply to this thread Reply
they are done as a function of frequency where:

f = W/2Pi
jaz

Posts: 25
Registered: 04/17/10
Re: PNA Measures as function of Angular Frequency or Frequency?
Posted: Jun 28, 2012 10:23 AM   in response to: daras in response to: daras
Click to report abuse...   Click to reply to this thread Reply
Hello daras,

Thank you for the reply. So the S Parameter data displayed on S21 is as function of frequency or angular frequency?

Thank you

Regards
Poh Lian
daras


Posts: 920
Registered: 12/01/05
Re: PNA Measures as function of Angular Frequency or Frequency?
Posted: Jun 28, 2012 10:51 AM   in response to: jaz in response to: jaz
Click to report abuse...   Click to reply to this thread Reply
Yes - when you setup a standard channel with sweep type set to linear or log frequency, then the independent variable on the x-axis of the displayed s-parameters is frequency.
Dr_joel


Posts: 2,763
Registered: 12/01/05
Re: PNA Measures as function of Angular Frequency or Frequency?
Posted: Jun 28, 2012 12:56 PM   in response to: daras in response to: daras
Click to report abuse...   Click to reply to this thread Reply
where the measure for frequency is cycles/second, or Hz (not radians/sec).

Point your RSS reader here for a feed of the latest messages in all forums