Contact an Expert

Thread: 83650L output level failure


Permlink Replies: 2 - Pages: 1 - Last Post: Jun 28, 2012 10:57 AM Last Post By: dhamilton
ADSuser

Posts: 1
Registered: 02/27/12
83650L output level failure
Posted: Feb 27, 2012 5:55 PM
Click to report abuse...   Click to reply to this thread Reply
Hi,

I have a problem with my 83650L synth. It seems to be ok up to 20.000 GHz but from 20.001 GHz and up the output power is unleveled and drops down significantly. At 20.001 GHz max output power is about -14 dBm and it goes down to below -100 dBm at 40GHz. The built-in selftest says that everything is working properly, but obviously this is not the case. I have access to the trouble shooting guide and the service guide for the 8360 sweeper series but i would appreciate any good ideas where to start looking for this failure. My initial guess after having a look at the block diagram is that it could be one of the amp/multiplier modules on the RF DECK, but this is so far just a guess. I have not measured anything yet. I hope the very abrupt power drop above exactly 20.000 GHz could be a hint what the problem might be for some person experienced with repairing 8360 sweepers.

Many thanks in advance for any help

Peter
tabbott


Posts: 1,483
Registered: 07/24/09
Re: 83650L output level failure
Posted: Feb 28, 2012 10:53 AM   in response to: ADSuser in response to: ADSuser
Click to report abuse...   Click to reply to this thread Reply
Hi Peter -

Your amp/multiplier module guess is correct.

83650L has different frequency bands that switch to different YIG oscillator harmonics to get the higher frequencies...
20 GHz to <26.5 GHz switches to the YIG 4th harmonic; RF out should be +10 dBm
26.5 to <38 GHz it switches to the 6th YIG harmonic; RF out should be +5 dBm
38 to 50 GHz it switches to the 8th YIG harmonic; RF out should be +2.5 dBm

Regards -
dhamilton

Posts: 145
Registered: 02/01/08
Re: 83650L output level failure
Posted: Jun 28, 2012 10:57 AM   in response to: ADSuser in response to: ADSuser
Click to report abuse...   Click to reply to this thread Reply
Peter,

Your RF doubler, 5086-7607 is bad. It requires repair.

Point your RSS reader here for a feed of the latest messages in all forums