Contact an Expert

Thread: Help about AC simulation.


Permlink Replies: 1 - Pages: 1 - Last Post: Jun 26, 2012 3:59 AM Last Post By: traducere simul...
littlemage78

Posts: 1
Registered: 06/09/12
Help about AC simulation.
Posted: Jun 9, 2012 9:48 AM
Click to report abuse...   Click to reply to this thread Reply
When I do AC simulation, from the simulation results, get a parameter named SRC. So who can help tell what's this mean? Thanks!
traducere simul...


Posts: 2
Registered: 05/23/12
Re: Help about AC simulation.
Posted: Jun 26, 2012 3:59 AM   in response to: littlemage78 in response to: littlemage78
Click to report abuse...   Click to reply to this thread Reply
The parameter src is the name of an independent source to which input noise is
referred to. The parameter type can be either dec, oct or lin, which specifies logarithmic,
octave, or linear distribution of frequencies, respectively.
The parameter nb specifies the number of frequency points per decade, octove or total depending on the value of the type
AIM-Spice Reference Manual, v4.0a 7
August 2004 parameter. fstart and fstop are the start and stop frequencies in Hertz, respectively.
pts_per_summary is an optional integer, if specified, the noise contributions of each noise
generator is produced every pts_per_summary frequency points.

For further info: http://homepages.rpi.edu/~sawyes/AIMSPICE_TutorialManual.pdf

Point your RSS reader here for a feed of the latest messages in all forums