Contact an Expert

Thread: LA sw bug ?


Permlink Replies: 4 - Pages: 1 - Last Post: Jun 22, 2012 7:15 AM Last Post By: Alx Threads: [ Previous | Next ]
Alx

Posts: 20
Registered: 12/28/11
LA sw bug ?
Posted: Jun 15, 2012 12:53 AM
Click to report abuse...   Click to reply to this thread Reply
I found in LA sw v5.30 it is not possible to store-recall by Setup Config or Setup&Data (.ala)
an External Trigger Output setting, if "Feedthrough" mode activated - is it correct functionality ?
"Polarity" setting is has no problem of that kind. 16902B frame...

It is not convenient to go every time to Setup -> External Trigger Menu, and change it manually!

Edited by: Alx on Jun 15, 2012 10:48 AM

Edited by: Alx on Jun 15, 2012 10:49 AM
algoss


Posts: 637
Registered: 11/03/06
Re: LA sw bug ?
Posted: Jun 15, 2012 4:08 AM   in response to: Alx in response to: Alx
Click to report abuse...   Click to reply to this thread Reply
Which LA cards? Please post screen shots of the setup windows, and any windows that change (before & after), so that this can be recreated.

You might want to call your local Technical Call Center. It's free and they can walk through the process with you.

Al
Alx

Posts: 20
Registered: 12/28/11
Re: LA sw bug ?
Posted: Jun 16, 2012 3:17 AM   in response to: Alx in response to: Alx
Click to report abuse...   Click to reply to this thread Reply
Some pics attached. 2x16950B-64 module used (1x16950B-64 configuration has the same problem).

I think that is some bug of LA software, External Trigger setting is not saved to Setup configuration.
algoss


Posts: 637
Registered: 11/03/06
Re: LA sw bug ?
Posted: Jun 21, 2012 12:40 PM   in response to: Alx in response to: Alx
Click to report abuse...   Click to reply to this thread Reply
Yes, it's a bug, and has been entered into the system for repair,

Additional settings were added to the External Trigger configuration window a few revisions ago, and through an oversight, those settings were not added to the configuration file. When you load a file, nothing is loaded for those setting, so they revert to the defaults.

It will be repaired at some point, but I don't have a planned date.

Al
Alx

Posts: 20
Registered: 12/28/11
Re: LA sw bug ?
Posted: Jun 22, 2012 7:15 AM   in response to: algoss in response to: algoss
Click to report abuse...   Click to reply to this thread Reply
Thank you very much!

Point your RSS reader here for a feed of the latest messages in all forums