Contact an Expert

Thread: UNIX - System Security Problem Detected


Permlink Replies: 2 - Pages: 1 - Last Post: Jun 22, 2012 6:32 AM Last Post By: oconnellj Threads: [ Previous | Next ]
david lim

Posts: 17
Registered: 06/20/12
UNIX - System Security Problem Detected
Posted: Jun 20, 2012 8:15 AM
Click to report abuse...   Click to reply to this thread Reply
Hi Guys,

I have met one problem with unix controller systems, after boot testhead and type "testhead is 1", it comes out "system security problem detected".
It cause operator based mode can't be displayed on the system.

Please refer attached details of the problem

I'm appreciate if anyone can help.

Thanks

Regards,
David
oconnellj

Posts: 95
Registered: 03/06/09
Re: UNIX - System Security Problem Detected
Posted: Jun 22, 2012 6:07 AM   in response to: david lim in response to: david lim
Click to report abuse...   Click to reply to this thread Reply
Hi David, on the screen it has 'testhead is1 and not 'testhead is 1'

one thing to try from a unix shell window is to use the command boot 1, (that is boot space one)

and see what happens

thanks, Jon
oconnellj

Posts: 95
Registered: 03/06/09
Re: UNIX - System Security Problem Detected
Posted: Jun 22, 2012 6:32 AM   in response to: oconnellj in response to: oconnellj
Click to report abuse...   Click to reply to this thread Reply
David, one more question - at what software revision are you at ?

Point your RSS reader here for a feed of the latest messages in all forums