Contact an Expert

Thread: Virtual Panel for U2000A USB Power sensor in VEE


Permlink Replies: 1 - Pages: 1 - Last Post: Jun 28, 2013 4:21 PM Last Post By: matthew_rose
steveor

Posts: 25
Registered: 09/25/09
Virtual Panel for U2000A USB Power sensor in VEE
Posted: Jun 19, 2012 10:46 AM
Click to report abuse...   Click to reply to this thread Reply
Hi,

I visited the agilent web site:
http://www.home.agilent.com/sec/techSupport.jspx?pid=1079918&pageMode=DS&cc=US&lc=eng&pselect=SR.PM-Search%20Results.Drivers,%20Updates%20%26%20Examples
And downloaded the virtual panel for the U2000A USB power sensor. This nice utility allows me to communicate with my USB power sensor. The only problem is, the virtual panel is offered as a secure runtime version (.vxe). It would be quite helpful to have the source code for this example. Can I get the .vee version? Without this, the utility only shows it is POSSIBLE to communicate with the sensor, but it would be much better to have the source code so I can follow this example in detail. Then, I could modify the code and use this in my application.

Thanks,
Steve Ortiz
matthew_rose

Posts: 10
Registered: 06/28/13
Re: Virtual Panel for U2000A USB Power sensor in VEE
Posted: Jun 28, 2013 4:21 PM   in response to: steveor in response to: steveor
Click to report abuse...   Click to reply to this thread Reply
Feel free to contact me at bid_support@agilent.com if you have any further questions on VEE and USB average sensors. Also please try out the free Power Panel N1918A software if you haven't yet.

Point your RSS reader here for a feed of the latest messages in all forums