Contact an Expert

Thread: Error running any example program on E4445A over GPIB in LabView


Permlink Replies: 1 - Pages: 1 - Last Post: Jun 14, 2012 7:54 AM Last Post By: mmich Threads: [ Previous | Next ]
mmich

Posts: 2
Registered: 06/14/12
Error running any example program on E4445A over GPIB in LabView
Posted: Jun 14, 2012 7:09 AM
Click to report abuse...   Click to reply to this thread Reply
Attachment pic_error.png (11.4 KB)
I keep getting the same error no matter what example program I run with the E4445A PSA. (Attached is a screen shot of the error window.) When I run the measurements manually everything functions as expected, however when I automate it with labview I get the following errors:

Possible reason(s):

Instrument reports:
+622,"External reference missing or out of range"
+101,"Frequency Reference Unlock"
+0,"No error"

Any help would be greatly appreciated, thanks.

mmich

Posts: 2
Registered: 06/14/12
Re: Error running any example program on E4445A over GPIB in LabView
Posted: Jun 14, 2012 7:54 AM   in response to: mmich in response to: mmich
Click to report abuse...   Click to reply to this thread Reply
Fixed. Had to tell it there was no external reference since there is only one input.

Point your RSS reader here for a feed of the latest messages in all forums