Contact an Expert

Thread: Yokogawa WT130 on 82357B GPIB


Permlink Replies: 0 - Pages: 1 Threads: [ Previous | Next ]
rsriram22

Posts: 1
Registered: 06/12/12
Yokogawa WT130 on 82357B GPIB
Posted: Jun 12, 2012 9:09 PM
Click to report abuse...   Click to reply to this thread Reply
What's the best way to control WT130 that is connected to the 82357B GPIB.. Tried using IIviPwrMeter, but i cannot set a few configuration options.. I need to be able to do it using Visual Basic 6.. I was looking at IIviPwrMeter.Measurement.Configure class, but not many options are available there....

I have 2 more of the 34970A's connected to the same GPIB and there is a easy way to control these using IVI.. I just have not been able to figure out a way to get to talk to WT130..

Alternatively, is there a way to send the SCPI instrument commands directly like "CONF:CURR:RANG" or "CONF:WIR"

Thanks

Point your RSS reader here for a feed of the latest messages in all forums