Contact an Expert

Thread: Error 2066 Corrupt Files


Permlink Replies: 3 - Pages: 1 - Last Post: Jun 14, 2012 11:38 AM Last Post By: Ballschmieder
Ballschmieder

Posts: 18
Registered: 05/13/10
Error 2066 Corrupt Files
Posted: Jun 12, 2012 8:18 AM
Click to report abuse...   Click to reply to this thread Reply
I had to remove my N5230A hard drive and after re-installing it files which I could previously recall, I now cannot. When I try I get Error 2066, corrupt file. I've tried loading back up copies of the files and get the same error. Is there something I'm doing wrong?
I've attached one of the files I'm trying to open.
jvall

Posts: 530
Registered: 12/08/05
Re: Error 2066 Corrupt Files
Posted: Jun 12, 2012 10:22 AM   in response to: Ballschmieder in response to: Ballschmieder
Click to report abuse...   Click to reply to this thread Reply
I have to admit that does not make much sense. I can't recall it either, so it does look like it may be corrupt. I will have to look into this a bit more and see exactly what got corrupted
johanericsson

Posts: 79
Registered: 03/07/07
Re: Error 2066 Corrupt Files
Posted: Jun 12, 2012 4:53 PM   in response to: Ballschmieder in response to: Ballschmieder
Click to report abuse...   Click to reply to this thread Reply
What version of the PNA firmware are you using to try to load the file?

The file requires there to be a source named MXG configured in the system. You should be able to configure a source named MXG - and then try again. (Although I see a problem with the recall when using the latest versions of the firmware)
Ballschmieder

Posts: 18
Registered: 05/13/10
Re: Error 2066 Corrupt Files
Posted: Jun 14, 2012 11:38 AM   in response to: johanericsson in response to: johanericsson
Click to report abuse...   Click to reply to this thread Reply
Yes, adding MXG got rid of my problem. However, would you expand on your comment "(Although I see a problem with the recall when using the latest versions of the firmware)"?

Point your RSS reader here for a feed of the latest messages in all forums